alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Presenting the Next Small Thing in Fluid System Optimization

 Small Bore Comparison 

 

Swagelok's popular Small-Bore Solution is a high-efficiency fluid system that reduces leaks, simplifies installation, and increases safety. Here's the what, why, who, where, and when behind it:

What is the Swagelok Small-Bore Solution? 

The Swagelok Small-Bore Solution is designed for fluid-system installations less than or equal to 2 inches in diameter.

Why should you use the Swagelok Small-Bore Tubing System?

The system can significantly save you time, money, and risk. 

Who can realize optimized safety and performance with the Swagelok Small-Bore System? 

Anyone using threaded or welded pipe is an excellent candidate for the Small-Bore system. 

How does a Swagelok Small-Bore System work?

Our solution consists of unparalleled, remakeable, leak-tight Swagelok Tube Fittings and premium-quality Swagelok bent tubing.  This combination requires far fewer system connections – and that means dramatically less dangerous and costly leakage – versus threaded or pipe systems.

Where else will I see labor/budgetary savings?

No longer required:  qualified welders, welding equipment and permits, fireboxes, air tests, tacking, purging, inspections, fumes, oils, gases, tape, pipe stands, dies, sealants, and SO much more.  In fact, you can assemble our system 50% faster and disassemble/reassemble it in 75% less time than competitive offerings.

When can I get a Swagelok Pittsburgh | Tri-State Area Rep to call or visit me?

NOW!


Contact us at info@pittsburgh.swagelok.com or 412.761.3212.